Belongs to this thread:
e2e.ti.com/.../opa380-can-opa380-used-to-amplify-the-photodiode-which-is-illuminated-by-a-dc-light
Kai
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Belongs to this thread:
e2e.ti.com/.../opa380-can-opa380-used-to-amplify-the-photodiode-which-is-illuminated-by-a-dc-light
Kai
Hi Kai,
Thanks very much for this informaton. Actually, it does work when amplifying a AC photocurrent now with 10kOhm, 100 kOhm and 1 MOhm, with or without a feedback capacitor. But this is not what I want.
What I am trying to amplfy is a DC photocurrent. The Phodiode is shined by a light with constant light intensity emitted from a LED.
I used different constant light intenisties (thus corresponding to different DC photocurrent values), but always get the same voltage output from the TIA.
That is why I am wondering a DC photocurrent can be amplified by the OPA380 or not. DC means the frequency is 0 Hz.
Best Regards
Yuefei
Hi Yuefei,
I understand what you mean. But even if only DC operation is desired, the OPAamp circuit must be designed to work stably. You will not get stable DC performance with an instable design. So please add the phase lead capacitance in the feedback loop and the isolation resistor at the output
Kai