Other Parts Discussed in Thread: LM358B, LM358,
The offset voltage of the LM358 shows only have positive value 3mV max, but the LM358B shows have negative and positive value, +/-3mV. My question are,
- Is the LM358A only have positive offset voltage?
- If the LM358B have +/-3mV Vos, so the possible Vos range is 3mV-(-3mV)=6mV. It means the LM358B has bigger Vos than LM358A. is that correct?
BR,
Gary