I want to measure output voltage of a DC/DC converter of 3.5kV for input to ADC of microcontroller. Could I use AMC1311-Q1 for this purpose? This IC requires 0-2V as input, so I have to use large voltage divider to scale the high voltage of 3.5kV to 2V. Would there be any problem in doing this? Are there other options available for isolated voltage sensing of such high voltages? Thank you.