This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMC662: Measuring the voltage from a very high Input Impedance Source

Part Number: LMC662
Other Parts Discussed in Thread: LMP7721

Dear Team,

We need to measure the voltage from a charge pump that is present inside the ASIC.

The Impedance of the charge pump is 200T Ohm. The team has designed a circuit with LMC662A which has an input impedance of 1Tohm.

Since the Impedance of Opamp is very less compared to the source, it will load the source. May I know the below circuit will be able to measure the voltage properly?

BOOT_STRAP.TSC

Regards

HARI