Hello guys,
One of my customers is considering using OPA551 for their new products.
They have a few questions about OPA551 as the follows. Could you please give me your reply?
Q1. The device datasheet (Version SBOS100B) says that RthetaJA of KTW(DDPAK/TO-263) is 22.7 degree /W in section 6.4.
Also it says that RthetaJA of KTW(DDPAK/TO-263) is 65 degree /W in section 10.3 . power dissipation.
Which is thermal information correct?
Q2. In 10.2 Layout Example section, PDIP-8 NC pins are connected to GND.
Is this no problem? Is this correct?
Your reply would be much appreciated.
Best regards,
Kazuya.