Other Parts Discussed in Thread: INA2181, INA240
Hi team:
Now we have problem at INA2818 application.
We use INA2181 for solenoid high side current amplifier at automotive product, the SCH like this.
The INA2181 have two failure modes:
- The output have 0.2V~0.8V offset voltage at the solenoid switch off status. This failure mode is our main problem. We have total 12pcs failure parts and all during sample building.
- The output voltage can't linear with input current, the input is 1.8A and the output is 0.8V. This failure mode is only one part at life testing. The solenoid is burning cause the driving current too high than needed.
Now we can reproduce the failures by ESD testing. But the failure mode is not same as our product. The ESD testing failure are combine 2 failures and only have failure 1(with offset output). You can find the result below, the INA2181 have 1V static output offset and not linear with input current at operating.
Could you pls help me to analysis the failure reason? And give me the troubleshooting suggestion. Thank you!