Other Parts Discussed in Thread: TLV3701, TLC277, TLC271, TLC272, TLV271, TLV272, LM358
I am using a 741 as a simple comparator. Supply voltage 10V. The input voltage range is low and must be variable between 0.8V and 2.5V. I suspect the 741 is not suitable for such low levels because below about 3V, the trigger point does not track the reference and bottoms out at about 1.9V. Am I correct? If the 741 is not suitable, what would be a suitable IC for this application?
Many thanks,
John Ogborne