Other Parts Discussed in Thread: ADS8568, OPA2156
Hey everyone,
First time really going in depth with analyzing the oscillations/instability due to the input stage of a SAR ADC. At this point I've gone through about 3 buffers and now I'm using the LM8272 which should be able to drive any capacitive loading. Am I incorrectly simulating this or misunderstanding what the behavior should look like?
I'm posting images with the isolation resistance at the output of the buffer, however removing/adding it does little to the initial drop in output.
Here's the circuit. I'm reading in a clean 5V DC signal, followed by an ISA which conditions the signal slightly. This is followed by the buffer to drive the input of the ADS8568.
At the output of the ISA, small oscillations/dips are already present
The output of the buffer does not look great, I was expecting something a little more "steady". If this is normal behavior, an explanation would be very appreciated.
Lastly, here is the output of the buffer overlaid with the voltage of the SAR ADC's sampling capacitor.
Am I missing something/ doing something incorrectly or is this not what this signal should look like.. Any help will really be appreciated