Hi, TI expert
I have an inquiry regarding the TL103WA.
Please inquire as the maximum rating for the entire pin is not shown on the datasheet.
1. When Vcc = 5V, can I check the Maximum Voltage Range and Maximum Current Range for each Pin?
2. Do VID and VI in the Absolute Maximum Ratings table mean IN pin(2,3,5,6pin)?
3. If you look at 1. Features on page 1 of the Datasheet, there is a content of "Large Output-Voltage Swing.. 0V to Vcc-1.5V". Can you explain in detail what it is?
Please confirm. Thank you.