Hi,
I have a number of IC's in small portable amplifiers that are faulty but I'm having trouble with identification of the device type.
They are micro smd 9 bump devices and I suspect they are class D 2w single channel audio amps.
The type markings appear to be:-
95W 17S
BP 27
Although the top line does vary the BP 27 is consistent. Due to the size of these devices it's difficult to see the markings clearly. I have checked through the data sheets for all devices of this type and can't find anything that would match these codes.
Could you possibly tell me if it is a TI device and if so what LMxxxx it might be?
Many thanks
Bob