Hi,
My customer is designing the software of the TAS5421.
They have questions about the diag resistor(0x02) read timing.
1. The figure 11 on the datasheet is mentioned the Load Diagnostics Sequence of Events.
When should they read the resistor(0x02)?
Should they read it after these events, or after check phase, or another timing?
2. And it is mentioned that "the check phase repeats up to 5 times" on the datasheet.
Does it mean that these events take 429ms(=75ms+52ms+50msx5+52ms) if the fault is present?
Please let me know lack of the information.
Thanks and Regards,
Kuramochi