Other Parts Discussed in Thread: LM1875, LM3886, TLC04, TPA3118D2
I have designed a TPA3118 board to use as a PA amplifier. The power supply is a 24 VDC, 3 amp unit. There is a transformer connected to the amplifier output that steps the voltage up to 70 volts. The transformer primary is 8 ohms and the secondary is 330 ohms. This translates to 15 watts at 70 volts.
I connect a 300 ohm load to the transformer secondary and drive the amplifier with a 1 kHz sine wave. I can drive the amplifier to full power for an extended period of time (over 15 minutes) and it continues to function properly. Testing with the signal generator, the output varies from 68.6 volts at 300 Hz to 74.4 volts at 15 kHz.
However, when I connect the voice announcement input source to the amplifier, I have problems. If the output exceeds roughly 7 or 8 watts, the amplifier goes into shut down. It will cycle back on after about 5 seconds. But continuing to make the voice announcement, the amplifier will re-trigger the shutdown cycle. Also, the source is switched into the amplifier input with a relay. If the volume level is set for more than about 8 watts output, the amplifier goes into shutdown when the source is switched on. Again, it comes out of shut down after about 5 seconds.
If I remove the transformer and connect an 8 ohm, 50 watt resistor to the amplifier, I do not experience the shut down issue. In fact, with the voice announcement source, I can drive the amplifier to 30 watt peaks with no shut down problems. Driving the amplifier with a 1 kHz sine wave to 30 watts for 15 minutes, there is no shutdown.
The transformer works fine with a class AB amplifier (LM1875 and LM3886) with the voice announcement input source. Using the LM3886, I can load the transformer secondary with 200 ohms (25 watts), drive it with a 1 kHz sine wave, and the output looks fine on my scope. So I don't think transformer core saturation is an issue.
I am using 10 uH inductors and the same resistor, capacitor values as shown in Fig 27 of the data sheet for the PBTL sub woofer circuit. But there has to be some kind of inductive kick back from the transformer that causes the TPA3118 to shut down.
Any suggestions will be appreciated.