Part Number: TPA3128D2
Other Parts Discussed in Thread: TPA3132D2, TPA3118D2, TPA3116D2, TPA3130D2, TPA3131D2
I'm having some issues with a new TPA3128D2 implementation when using 1SPW mode. When powering the device on (with open inputs) i can hear a clicking sound on the outputs which refers to stepped bias response on the inputs.
IC is configured as:
600kHz 1SPW
SE input (ground refered)
2u2F input coupling caps
1s power on mute
Weak 100k "pulldown" resistor to GND on the inputs before coupling-caps
System overview:
The clicking noise looks like this on power on:
Touching the inputs while powered on also results in clikcing noise as shown here:
As said, this isn't noticeable when using BD modulation. Any ideas?
Best regards,
Christian
www.360customs.de