Other Parts Discussed in Thread: TAS5721, , PCM3168
Dear Experts,
I´m a little bit confused about the EVM setup for theTAS5721EVM which might be the reason why I hear no sound on phono or speaker outputs.
First of all I do not find any matching documentation to my brand new "PurePath Console Motherboard AIP006G". All I found is some documentation for older hardware versions( Feb. 2015) . After some investigations and asking in this forum I download the PurePath SW Version 1.16 and load the TAS5721_PPCMB target. This was not documented but I got this information in this forum. In this case I assume I load the right target which hopfully match my hardware version of the PurePath Motherboard. In fact the hardware has more I/O than I can select/see at the block diagran which is shown by the selected target.
Nevertheless I check if a simple analog audio input can be heard by the PurePath Phono out which should me indicate if the selected targte is working. The audio can be heard by USB input and Analog input so I assume I´m working with the right target now.
The next step is to check the TAS5721EVM board´s major functionality. Unfortunately the displayed block diagram is different to the document ( june 2013). I do not change anything and so I assume that the audio signal which is processed successfully at the PurePath board is routed to the TSA5721EVM. I connect two speakers and a headphone but there is no sound. I try several settings but never get any sound out.
The target of the evaluation is to set up a 2.1 System which should be simple to set up. But If I switch the radio Button "mode" at the PurePath Software nothing changed at the block diagram. I assumed that the 3ch will be enabled.
I´m sorry but all documentation is quite old and do not reflect the current state. The EVM setup is not working in a basic configuration. This is not what I expect and not what was promissed "Simply graphical setup"
Nevertheless: I assume the setup will work but it seemed that there is some undocumented software or special cconfiguration setups are necessary.
Please be so kind and provide me a documentation how to bring the EVM system alive and how to setup a 2.1 system using the TSA5721.
Thanks a lot for your support in advance
Karsten
P.S. I´m sorry for my bad english...