Hi folks,
Customers measure THD+N but they are not sure the value is reasonable or not.
Below is what they measured:
SPEC: VDD = 5V, THD = 1%, Po = 1.46W, Vrms = 3.41V
Result: Vrms = 3.41V, THD = 1.72%
SPEC: VDD = 5V, THD = 10%, Po = 1.8W, Vrms = 3.79V
Result: Vrms = 3.79V, THD = 11.53%
Do you think this result is normal?
Thank you.
Regards,
Will