This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPA3116D2: TPA3116 Power Ratings

Part Number: TPA3116D2


On your page TI dot com /product/TPA3116D2

Are the watt (W) ratings RMS or something other?

I ask because the Output power line just says "Output Power(W) 50"

  1. Is this "W" RMS? If it's RMS then why does the PBTL line state "W(max) 100"?
  2. The TPA3116 has 4 amps in it, 2x two BTL's, or stereo output, so is one TPA3116 a 2x50 package?