Hi,
We use TPA3255 amplifier IC in PBTL mode for 300W output power. The frequency response that we got was not upto the bandwidth of audio frequencies. We got frequency response BW from 40Hz to 30khz instead 20hz to 20khz.The higher cutoff frequency is fine and we dont have any issue in that. But at lower frequency we need to improve it to 20Hz.Here are the specifications: Pvdd(V)=35Vdc, Lout=11uH(MA5172-AE),Cout(2caps in parallel)= 1uH(MKP4-1.0/250/10) & 0.47uH(MKP4D034704D00KSSD),Load impedence = 33.3ohm. Kindly help us and reply ASAP.