This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Linux/TAS5733L: Volume table implementation registers

Part Number: TAS5733L

Tool/software: Linux

Hi,

I am using TAS5733l Amp, for implementing volume table when i try to write on 0x07 (master volume reg) register, which following 

0x0000 24.000
0x0001 23.875
... (0.125 dB steps)
0x03FE –103.750
0x03FF Mute

This table. my speaker output is stopped even on 5 db onward. do we need to write on other register also except this. so i can implement volume table. please suggest this

example will be more helpful if you can provide.

Thanks,

Nikhil