Hello,
We have a question about INA181.
Is there any problem with the following condition?
We think that it satisfy the Absolute Maximum Ratings.
Vs(6pin) = 0V
GND(2pin) = 0V
REF(5pin) = 0V
IN+(3pin) = 24V
IN-(4pin) = 23V
In this case, how many voltages is OUT(1pin) ?
Will OUT(1pin) be 23V or 0V?
Best Regards,
itabi