I have an application which requires after startup the system to be brought down to -55C ambient temperature. Are there expected failure modes in this operating condition? I understand characterization of performance will need to be evaluated as we would be operating outside of specified rated temperature. Prior to moving forward with the preliminary design I would like to confirm if there are any known issues with low temperature operation that would possibly cause the device to not only stray far from specified performance during normal conditions but to cease functioning or some other failure that would cause no useful feedback to my system to occur.
Thanks,
Justin Samstag