This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA240: Low Side Current Measurement

Part Number: INA240

Hello dear support team, 

Could you please help me in answering the following questions:

  • How big is the input impedance of the INA240
  • Are Ref1 and Ref2 real Resistors? Which value do they have (there is no value in the datasheet)?
  • How is the PWM filter implemented (e.g. Cut-off frequency)?
  • Can it be compared with a standard EMI filter, but with bigger time constant to lower the cutoff frequency?
  • Can there be any problems, when the reference voltage can only source?

BR

  • Hello BTS,

    Thanks for reaching out on the forum. The Ref Resistors are real and as indicated in the figure below are roughly 50kΩ. Their tolerance is 15%, however they are trimmed to match.

    The common mode impedance is 500kΩ while the differential impedance is about 3.2kΩ. For calculating the common mode impedance, you take two point on the upper linear portion of the input bias current vs common-mode voltage plot. In this case I chose (20V, ~100μA) and (70V, 200μA). Thereupon you get the difference between these two points (50V, 100uA). Lastly, you divide your derived voltage (50V) from the derived current (100μA) to get 500kΩ.

    As for the differential impedance, you first take the difference in current between a point on the IB+ line and a point on the IB- line of the Input Bias Current Vs. Differential Input Voltage Plot. In this case I take values at a 1V differential voltage. So I get 240μA – (-70μA)=310μA. Thereupon I divide the differential (1V) by this difference (310μA), to get 3.2kΩ.

    The PWM rejection is more complicated than just an EMI filter. The design engineers took special steps on each stage of the INA240 circuit, to attain that special PWM filtering. As it involves the whole circuit, there is too much proprietary detail involved to share on the forum.

    As for using the ref pins as a source, what exactly were you planning on doing?

  • Hello BTS,

    I have not heard from you in a while, so I am going to presume that the above post answered your questions. However, if something was unclear or you need additional information, please post below.
  • Hello Patrick,

    Thank you for answering. I have been on vacation. The problem has been followed up internally within TI.