This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TL064: Isink/Isource

Part Number: TL064

Hi,

I would like to know the value of Isink and Isource of TL 064.

What is the minimun value of Isink and Isource?

Best regards,
Seishin

  • Seishin,

    The answer will depend a lot of the supply voltage(s) and output voltage.
    At what supply and output voltage do you need minimum current?
  • Dear Ron,
    Thanks for your prompt reply.
    I apologize for my lack of explanation.
    I need the minimum current of the following conditions.
    Vcc±=±15V,TA=25℃
    Vo=±2V and ±13.5V

    Best regards,
    Seishin

  • Seishin,

    For 13.5V the typical is 1.35mA for DS VOM spec (13.5V/10k). However this is close to the output headroom requirement. So the minimum current maybe close to zero. Especially if temperature wasn't 25C and was -40C (larger headroom).

    For 2V there is figure 3 in data sheet. 2V happens at 100 ohms which is a typical 2V/100 ohms = 20 mA. As a minimum my estimate is 14mA

    Why do you ask? I could help more, if I knew moore about the application.