Hi,
I'm wondering if I can use the TLV9062 to drive a low impedance load safely. E.g. 120 ohms
The data sheet shows output short circuit current as +/- 50mA, absolute maximum ratings, continuous short circuit. Can I use these figures to safely assume that, with a +/- 5V power supply, I can safely drive a 120 ohm load?
The second related question is, can I configure two amplifiers in parallel (from the same package) in order to boost the drive current? An example from another design using NJM4556 amps is shown below. The series output resistor is very low - 1 ohm. Would there be any obvious concerns with this configuration?
Regards,
ac