We are using LM211DR in one of our products.What I noticed is max voltage rating on input pin has a note #4 that restricts input voltage to be less than or equal to VCC in case VCC is less than 15 V. We are using VCC of 5 V. Our present design is applying 12 V on input which clearly exceeds the rating you have specified. We have not received any complain from field. I want know if the note # 4 in datasheet is valid or it is carry over from old datasheet.
Another reason for me to believe that the restriction is superfluous is that ON semi makes same IC and we have it in out list as an alternative but it does not have such restriction.