Hi,
I want to create amplifier, to amplify voltage from DC R Shunt. the voltage from r shunt is 0-60mV.
i want to amplifiy to 0-4.8V (80-81x gain).
i use TLV2472IDGNR, single supply +5V, and use R1 120K ohm R2 1.5Kohm (0805 1% tolerance)
configuration of op amp is non inverting.
The result of my trial, the gain was unstable, the gain is different between low voltage and higer voltage.
when i inject 5mV the gain was 60x, and the gain increase when the input signal increase. I try to inject 60mV the gain is about 77x.
could you please to help me, why it was happened, i try on ti web bench the result is like the calculation and the gain is stable.