Hello,
We have been using LMV931MF/NOPB, Package Code A79A. Suddenly, on a recent batch of these chips, we have been experiencing shutdown of the device.
Date code is: *75X
Inputs are connected to a photodiode receiver HCNR201 (Broadcomm), connected as:
Cathode (HCNR201 Pin 6) to Inverting Input (pin3)
Anode (HCNR201 Pin 5) to non-inverting input (pin1)
non-inverting input (pin1) to ground connection (pin2)
inverting input connected to output via 200K FB resistor + 0.1uF FB Cap)
Since HCNR201 is an isolation amp, the rails (pin5, pin2) are powered independently from the signal that is to the inputs.
When power is off (0V pins 5,2) the output signal drives to -0.3V
When power is ON (pins 5,2) the output responds normal (specifically 1.2V to 4.2V signal)
When power is removed and the reapplied between 200ms and 800ms, which is before the output signal drops below 0V, the output will remain locked at 0V.
IF Power is reconnected <200ms (before output goes low) or >800ms (after output goes to -.3V) the signal returns to normal.
Replacing the op-amp resolves the symptom.
This seems to only apply to op-amps with date code *75X
This may or not be related, as it is on a different board and chip, but may represent conditions seen by the chip described above:
We have a possible cause, in that the external interface 5V experiences considerable noise (greater than 5V Vcm, >2Vpp at times, around 200kHz for about 1ms)
During these events, our field engineer managed to capture this event on a scope, and roughly 10-20ns after the voltage exceeded 6V, the output signal dropped to zero. and the voltage between pin1 and pin3 was about 0.5V)
I am curious if there is an issue with a recent batch of these op-amps, if there is something that is causing these to drop-out, if there is damage occuring to these op-amps due to the voltage spikes that would cause this behavior, or anything you can think of that would be the cause.
Thanks!!