This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

I need a converter that is from 0.5-4.5V input to 4-20mA output

Prodigy 250 points

Replies: 1

Views: 452

I need a converter that is from 0.5-4.5V input to 4-20mA output,

could you recommend an IC? operation temp -40 to 120℃.

thank you.

Best regards

Weiming

  • Hello Weiming,

    Please consider the XTR115, XTR116, or XTR117 for this applications.  Guidelines to size the external gain-setting components can be found in the theory and component selection sections of the following reference design:  TIPD126

    Regards,
    Collin Wells
    Precision ADC Applications

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.