This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

Will asymmetric rails on the RC4558 effect the slew rate?

Genius 3245 points

Replies: 3

Views: 835

Hello,

Would using asymmetric power supplies (i.e +12 and -15V) on the RC4558 effect the slew rate?  I'm thinking since it can operate in single supply mode, it might not be a problem, but wanted to verify.

Thank you

  • Hello,

    There should be no change in the slew rate because of this.

    Best,
    Michael

    Have a question about Logic or Level Translation?
    Find answers through our Logic Support and Training Page

  • In reply to Michael J Schultis:

    Thanks for you help here,

    Just one follow up here.  Is there anything we should be concerned about in using asymmetric rails?  Will it go into compression or anything like that?

  • In reply to Jamaal_Charles:

    Jamaal,

    No problems like that.

    For +12V , -15V there is just a 3V reduction in some spec (relative to +/-15V)

    For example common mode range will be -12V to +9V instead of -12V to +12V.

    Regards,
    Ronald Michallick
    Linear Applications

    TI assumes no liability for applications assistance or customer product design. Customer is fully responsible for all design decisions and engineering with regard to its products, including decisions relating to application of TI products. By providing technical information, TI does not intend to offer or provide engineering services or advice concerning Customer's design. If Customer desires engineering services, the Customer should rely on its retained employees and consultants and/or procure engineering services from a licensed professional engineer (LPE).

     

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.