This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

LMP91000: Design

Prodigy 80 points

Replies: 4

Views: 942

Part Number: LMP91000

Hi. I'm making a prototype with which I'm going to sense Co2, C2H4 and O2 (the sensors are from alphasenser, 3 cells and 2 cells). At the moment I do not want to weld the PBC to the LMP91000 so I'm going to need a socket, my question is, which socket do you recommend for the lmp91000?

  • Hello,
    I believe that LMP91000 package (WSON-14) requires a custom order for the socket. TI can't recommend specific vendors since there are few in the market that could support your needs.

    Regards,
    Jose

  • In reply to Jose Arteaga4:

    Hello Jose,
    Which is the most common use of the lmp910? I mean, How I can test the LMP9100?

    Regards,
    Victor
  • In reply to user5179595:

    LMP9100 is a AFE (Analog Front End) to interface Gas sensors (electrochemical cells) on a topology known as Potentiostat Circuit.

    For more details please refer to the LMP91000 data sheet www.ti.com/.../lmp91000.pdf
    To evaluate the part you could order the LMP91000EVM: www.ti.com/.../lmp91000evm
    Alternatively there is a TI Design with MSP430 that you can refer and create your own: www.ti.com/.../tidm-1chp-dtect-co

    Regards,
    Jose
  • In reply to Jose Arteaga4:

    Ok. Thank you for you time.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.