This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

TINA/Spice/LMH6624: TINA TI

Prodigy 40 points

Replies: 6

Views: 282

Part Number: LMH6624

Tool/software: TINA-TI or Spice Models

Hello,

I have a little problem with simulating the LMH6624. I would like to use this device for an Butterworth filtter 4th order. The max frequency i want to work with is 1Mhz.

None of my tried applications seems to work so i've broke it down to the beginning and tried some standard non inverting circuit. 

The input Voltage is 100mV on 1Mhz. 

Why is the simulation going into something like a saturation, vice versa the voltage follower seems to work.. Did i miss something? I have no clue where my mistake could be =( .

I appreciate any help.

  • Hi Stefan,

    if you power the LMH6624 with a single supply voltage, you need to set a DC operating point like shown in figure 56 of datasheet.

    Kai
  • In reply to kai klaas69:

    Hi Kai, thanks for the fast answer! I've already tried this...and the output was the same as in my uploaded picture. additionally i've set an offset of 50mV to my input signal, because my later signal isn't an AC as well. I read something about an decompensation of the phase shifting, but I think i'm out of that range :/ maybe i'm wrong and that does matter to my application
  • In reply to Stefan Langlouis:

    Hi Stefan,

    can you post your TINA-TI file?

    Kai
  • In reply to kai klaas69:

    try1.TSC

  • In reply to Stefan Langlouis:

    the values are changed in this file. But ist doesn't work too. I think it has to be something with the Simulation program itself
  • In reply to Stefan Langlouis:

    Hi Stefan,

    if you use a single supply voltage, you must take care that the DC operating point is not amplified by the signal gain. So, you urgently need a high pass in the feedback loop, here introduced by C2:

    stefan.TSC

    Kai

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.