This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

AMC1100: AMC1100

Intellectual 380 points

Replies: 8

Views: 429

Part Number: AMC1100

We are working again on the same project  3Ph voltage measurement using AMC1100.As per attached functional block diagram.

Need to understand the effect of connecting to-gather mains neutral with AMC1100 input side GND. Considering the electrical noise of all three phase will return through the common neutral. 

3_Ph_Voltage_Sensing_AMC1100.pdf

  • Hi Amruta,

    what is your question?

    Kai
  • In reply to kai klaas69:

    Hi,I wanted to know
    1. Should I connect to-gather mains neutral with AMC1100 input side GND.
    2. What is the effect of electrical noise of all three phase which will return through the common neutral.
  • In reply to Amruta Bhujbal67:

    Amruta, hello. I noticed that you haven't received an answer for this design. Our apologies. Please advise if you still need assistance with your question regarding the AMC1100. In the meantime, I am going to loop in the design owner for the TIDA-01555, which I was advised you are asking about here.

    Best Regards,
    J. Fullilove
    Texas Instruments
    Reference Design Operations
  • In reply to Amruta Bhujbal67:

    Hi Amruta,

    yes, you can do this. And figure 37 of datasheet of AMC1100 shows an optional way to generate the supply voltage VDD1. But do not connect VINN directly to mains neutral. Instead use some input filtering, as shown in figure 34 and 39 of datasheet. Of course, use an individual input filter for each AMC1100.

    Kai

  • Hello 

    When multiple voltage are measured as group isolated measurement module, you will have to tie the neutral.

    The effect of noise depends on the layout and we have achieved 0.1% measurement accuracy from 5V to 280V.

    Thanks

    Sreenivasa 

  • In reply to JohnFullilove:

    Hello,

    Thank you for reply for post related to AMC1100.Yes I still need help with question regarding AMC1100.

  • In reply to Amruta Bhujbal67:

    Hello Amruta

    I am not sure what helo you are looking for.

    In case your question is on the noise effect, i do not see that affecting the measurement if you take care of the routing as per TIDA-00555 in your design.

    Thanks

    Sreenivasa 

  • In reply to Amruta Bhujbal67:

    Hi Amruta,

    there is no special noise issue, when connecting mains neutral to GND1 of AMC1100. This is the best you can do, anyway. But use the input filtering as mentioned in my last post:

    e2e.ti.com/.../2947793

    Kai

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.