THS4281: Use as comparator?

Prodigy 340 points

Replies: 1

Views: 36

Part Number: THS4281

Hello,

Does THS4281 have anti-parallel diodes on the input? Can it be used as a comparator?

Thanks,

Michael

1 Reply

  • Hi Michael, 

    The THS4281 has a maximum differential input voltage of 2V. Depending on your supply voltages and threshold, you might be able to use it as a comparator. However, it will have poor output recovery time compared to a dedicated comparator device. 

    Regards, 

    Jacob Freet 
    High Speed Amplifiers