I have a circuit where I am using an op-amp in a gain of 1 buffer condition. Rails are +12V and -0.237V (LM7705). My input signal is a voltage divider and can range between 10V (open circuit) and 50mV. Resistors change between the end of R9 (see below) and ground to give a variable voltage divider. I feed the voltage through a low pass RC filter which consists of a 100K resistor and a 0.47uF cap to ground on the +IN terminal on the op-amp.
My current part selection is the OPA2188. I would like to reduce the V+ rail to +10.4V. However the OPA2188 is not a rail to rail input part. I have been testing the LMV842, but I am getting errors as I approach 10V on the input (even with the original 12V V+ rail). Is there some effect with the internal diodes I am violating?