This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

What are OPA2379's bias and offset specification over temperature

Other Parts Discussed in Thread: OPA2379, OPA379

With OPA2379, we see a drift which appears to exceed the datasheet specifications.


What is the bias current specification over temperature? Datasheet says maks +-50pA but I think this is only specified at 25 oC. Right?


Are there any specified limits at other temperatures, because figure 14 is only for typical values. Right?

So how do we determine the limits for the bias current at other temperatures than 25 oC?

Her is a discription of our setup and our results:

The circuit is as simple as possible: A transimpedance amplifier with 0 A input current. This is to be taken very literally because the feedback circuit (R||C) is an air-connection. The node connected to the in- pin is in free air. The common mode is thus 1.25V below the Vs as recommended with regards to low offset voltage.

We measure the output voltage versus temperature. This is a measure of the combined input offset and input bias current, and of course any leakage currents which could be there as well. We checked that the circuit is stable. The circuit is in a metal enclosure as the in- node is very sensitive to electric field pickup.

Below 30oC the output voltage is generally below 1mV. But gradually raise to from 3mV to 4mV at 70oC.

Datasheet specifies:
Voffset <2mV over extended temperature range.
Voffset drift is maks 2.7uV/oC => or maks 0.10mV at 40oC change.
Ibias is maks +-50pA at 25 oC => 10Mohm*50pA = +-0.5mV
Ibias variation figure 14: indicate that the bias current should stay below 100pA = 1mV output change. (Is that true?)
So in total this never going to add up to 3 to 4mV. Where is the mistake?

Thanks for any hints you can provide.

Here are the relevant(?) datasheet extracts:

  • Henning,

    The typical input bias current, IB, specified in OPA379 datasheet is 5pA at 25C and according to Fig 14 becomes ~60pA at 70C (12x increase) so the maximum IB specified as 50pA at 25C could become 50pA*12=~600pA at 70C.

    Datasheet specifies the maximum input offset voltage, Vos, at 1.5mV at 25C but 2mV at 125C so the maximum drift is: (2mV-1.5mV)/(125C-25C)=5uV/C and not 2.7uV/C - the latter is just a typical spec.

    Therefore, as you change the tempearature from 25C to 70C the input offest may change by as much as 225uV (45C*5uV/C) while the voltage across the feedback resistor may change by: (600pA-50pA)*10Mohm=5.5mV

    Thus, as you change the temperature from 25C to 70C, the total Vout change may be as high as 5.725mV