I have a prototype board that uses an INA194 (SOT-23-5) to measure current from a high side shunt.
- Shunt - 0.012 ohms
- Current range - 0 - 5 Amps (0 - 60mV)
- Common mode voltage - 200mV to 48v (typical will be 1.5v to 48v)
I found that the sensor was terribly inaccurate with low common mode voltages and low Vsns, and then found that this is described in the datasheet. It looks like LMP8640HV-F (SOT-23-6) will just drop onto the footprint and work. Is there anything I'm overlooking that will make this not work?