Hi,
I need a transimpedance amplifier to connect output voltage of AC resistors (value from 10 mohm to 1000 ohm) to PXI 4461 that has 1 MΩ || 217 pF on the inputs. The frequency of interest is 50-100 kHz.
I am new to amplifiers, so I guess I need a unity gain amplifier (OPA656 looks good to me) conected as transimpedance amplifier. That looks simple, and I plan to use DEM-OPA-SO-1A to test everything. I know I don't need any resistor in the return path, but my question is do I need any other components (capacitors or resistors connected such as from positive to ground), etc...
And also, is OPA656 fit for purpose or is there any better amplifier to do the job. Is evaluation board DEM-OPA-SO-1A OK to test it?
Thanks for all the help
Neven