I have a linear TEC driver application that I need to source 10A with an output voltage very close to the VCC rail. The best solution I have found so far is to parallel 5 OPA569 devices. The datasheet shows 2 devices with device1-> parallel_out1 (pin2) connected to device2-> parallel_out1 and device1-> parallel_out2 (pin9) connected to device2-> parallel_out2.
Can anyone confirm the proper connection for more devices? Do I simply connect all of the parallel_out1 (pin2) pins together and connect all of the parallel_out2 (pin9) pins together or is there some other connection scheme like daisy-chain?
The datasheet indicates almost nothing about these pins and the load sharing circuitry. Does anyone have any indication of how these pins work internally?
Thanks,
Matt