This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

INA188 in TIDA-01063

Mastermind 7655 points

Replies: 5

Views: 695

Dear all.

TIDA-01063 measures an AC current, but can DC be gauged with the same Rogowski method?

Regards,
PAN-M

  • Hello PAN-M,

    A Rogowski coil requires a time-varying current. Can you please give us some information about your application? Perhaps there is another solution. I'm specifically looking for the common-mode voltage, available supply voltage(s), load current range/direction, and output voltage requirement.

    Regards,

    Pete Semig

    Applications Manager, General Purpose Amplifiers

  • In reply to Pete%20Semig:

    Pete
    Please regard as this application is welding machine.
    The current is more than 100A.
    The shunt registance is too hot, and by a usual coil, the performance is ill-balance.
    Regards,
    PAN-M

  • In reply to PAN-M:

    Hello PAN-M,

    Sorry, but I have some more questions:

    What is the common-mode voltage? What power supplies are available for the amplifier? What shunt resistance are you currently using? Can you please clarify what you mean by 'ill-balance'?

    Regards,

    Pete Semig

    Applications Manager, General Purpose Amplifiers

  • In reply to Pete%20Semig:

    Hi Pete,

    Our customer said;
    P-N voltage is 282V typical, but they don' t know grand-fault voltage.
    Also, they don't know grand-fault current.
    A power for the amplifier can be made because this is new design.
    The shunt registance is 2m-ohm, they use.
    They ware try to Hole method current sensing, but the coil ballance is bad.

    Regards,
    PAN-M

  • In reply to PAN-M:

    Hello PAN-M,

    If I understand the system correctly there are perhaps a couple solutions here. First, they may want to consider the INA149. Given dual +/-15V supplies it can accommodate +/-275V common-mode voltages. In this case you could use a single supply to accommodate for the larger common-mode voltage. Please refer to Figure 3 in the INA149 data sheet.

    Another option could be the AMC1200. It has a fixed differential gain of 8V/V and can accommodate very large common-mode voltages because it is isolated. If this interests the customer please let me know. The AMC1200 is supported by a different group and I can move this thread to the appropriate forum.

    I hope this helps.

    Regards,

    Pete Semig

    Applications Manager, General Purpose Amplifiers

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.