Hi
We are about to replace AD823 with TI product.
Additionally, we want to the following requirement.
- Input capacitance > 20pF
-Input resistance > 10Mohm
-Small package (smaller than 1.6mm x 2.9mm if possible)
We found the LMV861 and LMV881, but we can not get input resistance value on the datasheet.
1. LMV861 and LMV881 have Cin spec as follows
LMV861
Common mode input capacitance : 20pF
Differential mode input capacitance : 15pF
LMV881
Common mode input capacitance : 5pF
Differential mode input capacitance : 15pF
LMV881 has small value of common mode input capacitance than differential mode. Is that correct?
2. What is the input resistance of LMV861 and LMV881?
BestRegards