Other Parts Discussed in Thread: TLC27L9, LMC6044, TLC27L4
The TLV2404IDR output of the first op amp goes to rail (high) during low temperature (less than 10 degree Celsius). Is there someone in TI that can help with this issue?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Gilbert,
Yes, we can help.
Can you please provide more details (schematic, supply voltage, measured voltages, output load, etc), and preferably a scope photos and/or voltage measurements before and after the problem?
Regards,
Hello Gilbert,
Looking at the schematic and scope photos, most likely it is due to the fact that the TLV2404, which is a nano-power (900nA) op-amp, just cannot drive the feedback and output loads.
It has a very "weak" output stage (200uA max). It cannot drive "normal" ~20K loads full swing (and feedback resistors count as a load). Nano-power amplifiers are expecting feedback resistors and loads in the meg-ohm range (to minimize power dissipation in the feedback).
If you look at the output sink/source graphs in figures 15 and 16, you can see that the current limit kicks in at about 80-150uA at cold (worse sinking). Output drive drops with temperature. You are probably on the edge of operation and seeing the device-to-device variation.
The LT1491 is a much higher power amp (10uA), and is capable of sink/sourcing several mA.
Is there a particular reason you chose the TLV2404 - other than a micro power 12V quad?? The resistor sizes do not suggest a micro-power application.
Looks like you do not need R-R Input, so have a look at a device like the TLC27L4, TLC27L9 or LMC6044 - as these are <20uA and can drive several mA.
Regards,
Paul Grohe