Hi,
i want to use the INA170 to sense current in a 24V power supply.
The INA170 is supplied with 3.3V on V+. The 3.3V will start a few 10ms after the 24V is applied.
According to the datasheet, Vin+ and Vin- may be +40V, but only according to maximum ratings. Is it ok to use the 3V3 as supply, or do I need to use the 24V?
Using the 24V is problematic in my application: In case of overcurrent, i need extra protection for the ADC input.
Thanks for any help in advance!