Other Parts Discussed in Thread: TIPD129, OPA320, , INA213, INA138, INA139, INA225, INA169, INA168
Hi,
Our application requirement is as below and we are in need of a Current Sense Signal Conditioning/Amplifier for this.
Requirements-
Current Range - 1mA to 30A
Resolution - 1mA
We are using low side current sense for this as high side will lead to high common mode voltage. We plan to use a current sense resistor of 25mOhm to counter lowest current measurement. Doing the math for 1mA to 30A will lead to a voltage drop of 25uV to 750mV across the sense resistor.
1. Can you suggest a suitable Current Sense amplifier/conditioning to measure this differential voltage across the resistor?
2. Also, even with a highly precision Opamp, offset voltage tends to be in order of tens of uV. Our lowest measurement might me well below this offset voltage. Will this impact our application considering we will be calibrating this system before its use to nullify the offset error?
3. Are instrumentation amplifiers are required for this application or can this be achieved using a precision Current Sense?
Regards,
Mithun