So I have the LMH6629SDEVAL board, and I am just trying to turn the amplifier on to get some performance specs.
I did not physically alter any components on the board, so all of the resistor values and such are still to spec.
I did not alter the positioning of the switches, because the AppNotes ("User Guide") wasn't exactly clear on the modes determined by the positions of the two switches.
Switch A: open, Switch B: closed. "Normal Operation"
I am using an Agilent E5062A Vector Network Analyzer (VNA), I know how to perform a two-port calibration for the VNA.
I connected "IN +" to Port 1 of my VNA, and "OUT" to a 20 dB Attenuator. I left PD floating, which defaults to logic 1, turning the amplifier ON. I left COMP floating, which does not matter, (I think), because I am not looking for a gain above 10 V/V, based on the circuitry given.
I left "IN -" floating, because I was not sure what to do with that, which I am sure is part of my issue.
I am unsure if I should connect a dummy load (50-Ohm Load) to the inverting input of the Eval board, or leave it floating.
After all of my calibration, I hooked everything up, making sure I did not lose my calibration (oh, yeah, I calibrated for my VNA's full frequency range: 300kHz to 3GHz), turned on my power supplies,
and got a -50 dBm for S11, and something that was all around wrong-looking for S21.
(My goal is to figure out the amplifier's response as-is from at least 300kHz to around 750MHz (I am okay with poor response, I just want to see some data), and then do all of the stuff I need to, and re-test; I just want to make sure this board works, first)
I was wondering if anyone could tell an obvious mistake I had made, off the bat.
Thanks for reading this,
- Dillon