This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV8812: Op Amp - Recommendation

Part Number: TLV8812
Other Parts Discussed in Thread: TLV2760, TLV2450

Hello,

I looking for Op Amp, Similar to the TLV8812/11 characterises, with an enable pin, could you help me and recommend? 

best regards,

Shahaf

  • Hello Shahaf,

    The lowest power op-amp with a shutdown is the TLV2760 (28uA @ 500kHz), though it is 3.6V max. The next lowest would be the TLV2450 (42uA @ 220kHz, lower noise)

    The LPV/TLV8xx series were designed for always-on applications. The current is low enough it can easily be powered off a GPIO pin.