Hi,
There is a specific TI pdf that details an active pass band circuit using the THS4551.
Table 2 is on page 6. It lists R2 as feedback resistor and R3 as gain resistor. Table 6 is on page 9. It lists R2 as the attenuation resistor and R3 as the feedback resistor...?
Additionally, there is a circuit (figure 5 on page 6) that outlines R2 and R3 and the component values listed are mixed up from the info on Table 6 as well. Is this an error? I'm trying to use the formulas on page 8 to calculate my component values but I am getting confused reading this TI document.
I am no circuit whiz so I am unsure which resistors would control an overall op amp gain of 2500. I see the formula listed for pass band gain which depends on the ratio of the input and gain resistors. Is that different from the regular op amp gain that typically depends on the ratio of gain and feedback resistors?
If the pass band gain only refers to the shape of the filter then I do not necessarily want to increase that. I just want an overall op amp gain of 2500 and I'm not sure how to plug in my resistor values to do so.
Also if the pass band gain is a different than op amp gain, does it still add/multiply with the op amp gain or are they completely independent? Any help clearing this up is really appreciated!!