This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • TI Thinks Resolved

INA196: AC current sensing using INA 196

Intellectual 810 points

Replies: 2

Views: 679

Part Number: INA196

Hi,

The  INA196 have bandwidth of 500KHz according to the datsheet.
I need to measure the current on an AC rail with 12V @ 200KHz switching.

Q1. Can I use INA196 for this purpose?

Q2. If Yes, Do the circuit attached can be used for the purpose?

Thanks in Advance
DEEPAK V

  • DEEPAK,

    Is this a PWM signal, and is the duty cycle fixed at 50%?  Also, I'm assuming this AC signal is just jumping from 0 to 12V, not -12V to 12V, which would work for the device because it is only unidirectional.  However, there are a few things to know about the INA196 - first is that it is not recommended for use with Vsense<20mV (see this article).  If you expect to measure small sense voltages generated by current through that sense resistor, I would consider other products, like the INA240.  The INA240 is built for PWM switching signals, though it is not a linear amplifier so you might have a little trouble at 200kHz, especially if the duty cycle changes (see this article).

    I see you have a 75Ω sense resistor which means you're probably measuring small currents, yes?  What range of currents are you thinking?

    Best Regards,

    Jason Bridgmon, TI Sensing Products Applications Support

    Current Shunt Monitor Video Training Series

    Hall Effect Sensor Video Training Series

    TI makes no warranties and assumes no liability for applications assistance or customer product design. You are fully responsible for all design decisions and engineering with regard to your products, including decisions relating to application of TI products. By providing technical information, TI does not intend to offer or provide engineering services or advice concerning your designs.

  • In reply to Jason Bridgmon:

    DEEPAK,
    Haven't heard back from you in a while so I'll assume you solved any design questions you had regarding this application. If that's not the case or you have followup questions, please come on back and post again here or in a new thread and we'll get right back to you.

    Best Regards,

    Jason Bridgmon, TI Sensing Products Applications Support

    Current Shunt Monitor Video Training Series

    Hall Effect Sensor Video Training Series

    TI makes no warranties and assumes no liability for applications assistance or customer product design. You are fully responsible for all design decisions and engineering with regard to your products, including decisions relating to application of TI products. By providing technical information, TI does not intend to offer or provide engineering services or advice concerning your designs.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.