This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

THS6212: THS6212 problems

Part Number: THS6212
Other Parts Discussed in Thread: THS6214

Dear all,

when i use THS6212 to design PLC products,i met someting confusing. Problems as follows: The broadband carrier module generates heat when working, after basic testing, I fixed the position on THS6212, and it generates heat a lot.Then i did lots test about sample and found the short circuit between VCC and GND(the impendence between VCC and GND <100oum).The power supply VCC is about 12V, and the load current is about 50mA.The eletrical schematic as below,Pls give professional analysis and look forward to your repply!!!Thanks again!!