This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA126: single power supply problems

Part Number: INA126

Hi. I am having problems to use INA126 with load cell. My configuration is: Input common mode Voltage = 2.5V. Power Supply = 5V/0V. Vref = 0V. I would like to know the limits of Output Voltage I will have.

For example, on the picture below, I know that if I were using Vref = 2.5V it would be between 0.6V - 4.3V.

Thanks for any input about that.

  • Hello Frederico,

    The output limit for the INA126 with your specifications are from 800mV - 4.25V. 

    The INA tool I used to generate this trump plot can be downloaded from the attached link below in the software section.

    Best regards,


    Errol Leon
    Texas Instruments
    Precision Amplifier Applications Engineer

  • Thanks Leon!

    I did not know about this INA TOOL. I will use it to simulate other configurations.

    Probably what I need is to use symmetrical supply... I would like to Min Vout near real zero volt.

    Best regards.