This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA4170-Q1: Difference between OPA4170 and OPA41

Part Number: OPA4170-Q1
Other Parts Discussed in Thread: OPA4170, OPA4171

Hi champs,

My customer evaluated OPA4170 and OPA4171 with attached circutry.

As shown in attached file, when OPA4710 was applied, output sinsoidale waveform shows distortion, but OPA4171 works better.

Could you explain from design point of view, waht is major difference between OPA4170 and OPA4171?

Best regards,

  • Hi Nobuo,

    the OPA4171 is faster and has a stronger output. So, for me it's no surprise, that the OPA4171 looks better.

    Kai
  • Hi Nobuo,

    Both OPA4170 and OPA4171 are rail to rail CMOS amplifiers.

    The key differences between them are summarized below:

    OPA 4170

    OPA 4171

    GBW = 1.2 MHz

    GBW = 3 MHz

    Slew Rate = 0.4 V/us

    Slew Rate = 1.5 V/us

    Quiescent Current = 0.1 mA

    Quiescent Current = 0.475 mA

    Voltage Noise @ 1kHz = 19 nV/rtHz

    Voltage Noise @ 1kHz = 14 nV/rtHz

    Highlighted in yellow might be the root cause to distortion you're experiencing .

    From the above waveform:

    # Of Divisions per cycle = 2.5

    @ 20 us/div ; T = 50 us per cycle

    Frequency = 1/T = 20 kHz

    For OPA 4170:   V_Out_Peak=  (Slew Rate)/2πf=  (0.4 V/us)/(2*π*20kHz)=3.183 V_pk

    For OPA 4171:   V_Out_Peak=  (Slew Rate)/2πf=  (1.5 V/us)/(2*π*20kHz)=11.937 V_pk

    In your application, if you’re nearing 3 Vpk_output with OPA 4170 you may see distortion induced due to slew rate.

    Can you also please check that your output current is below the specification for both configurations? A quick way to check if this caused distortion is to increase the load impedance 10X to see if that fixes the distortion.

    Note: Since we are comparing similar amplifiers. General rule of thumb is Increase in Iq, Bandwidth, Slew rate; Decreases distortion and Noise.

    Best Regards,

    Bala Ravi

  • Ravi-san,
    Thank you very much for your dedicated response.
    Best regards,