Other Parts Discussed in Thread: THS4551, TIDA-01057
In THS4561 datasheet the THD is shown as
Very Low Harmonic Distortion
- HD2: –115 dBc at 2-VPP, 100-kHz
- HD3: –110 dBc at 2-VPP, 100-kHz
THS4551 datasheet
- HD2: –128 dBc at 2 VPP, 100 kHz
- HD3: –139 dBc at 2 VPP, 100 kHz
So it seems THS4551 is much better at least for 100kHz
TIDA-01057 showed THS4561 is slightly better than THS4551.
Not sure how to understand this.
Is there a THD or THD+N vs input freq curve data for TIDA-01057 design?
(THS4561 datasheet does not have THD vs input freq plots)
Thanks for the help!